Skip to main content

Your fridge and an air conditioner use the same technology, and understanding that connection shows why heat pumps are one of the most energy-efficient ways to heat a home

An air conditioner and a refrigerator both move heat rather than generate it, using the same cycle of refrigerant, compressor, and expansion valve. Because moving heat requires far less energy than creating it, a heat pump can deliver 3 to 4 units of thermal energy for every unit of electricity consumed. This article explains the shared science and shows how heat pumps are a cheaper and more sustainable way of heating and cooling your home

What is an air conditioner and how does it work?

The basic principle: moving heat instead of generating it

A heat pump is a device that moves thermal energy from a cooler place to a warmer one. It uses a small amount of electricity to power this transfer, but the heat it delivers is several times greater than the energy it consumes. In practice, a heat pump can typically provide three to four units of heat for every unit of electricity used. Because the system moves existing heat rather than generating it through combustion, it can deliver the same level of comfort while using far less energy than conventional fossil-fuel boilers, often translating into lower heating bills over time.

The system works through a continuous cycle involving four main components:

  • evaporator
  • compressor
  • condenser
  • expansion valve.

How the heating and cooling cycle works

In heating mode, the outdoor unit absorbs heat from the surrounding air. The compressor then raises the temperature of that energy so it can be released indoors through radiators. After the heat is delivered, the refrigerant cools, its pressure drops, and the cycle starts again. Most modern systems also include a reversing valve, which allows the same equipment to run the process in the opposite direction and provide cooling in summer. In practical terms, this means a single installation can provide both heating and cooling, replacing the need for separate heating and air-conditioning systems.

A common misconception is that heat pumps stop working in cold weather. In reality, even cold air still contains usable thermal energy. Modern refrigerants are designed to absorb heat at very low temperatures, allowing heat pumps to operate efficiently even in winter conditions. For homeowners, that means a single electric system can provide reliable heating year-round.

The common ground between air conditioners and refrigerators

The easiest way to understand a heat pump is to think about your refrigerator because they both rely on the same underlying refrigerant. If you stand behind a fridge while it is running, you can feel warm air coming from the back. That heat is the result of the appliance moving warmth from inside the cabinet and releasing it into the room. It's a straightforward process:

  • Evaporates → absorbs heat from food and air inside the cabinet
  • Compressed → pressure and temperature of the gas rises
  • Condenses → heat is released into the kitchen, refrigerant turns back to liquid
  • Expands → pressure drops, cycle resets

A heat pump uses this same method, but on a much larger scale to heat an entire building. Instead of removing heat from a small insulated box, it draws heat from the outside environment and transfers it indoors. Because this technology is based on a cycle that has been refined for decades in everyday appliances, heat pumps are less unfamiliar than they might first appear.

Innovations in refrigerants from a global perspective

Europe’s heat pump technology is advancing quickly, driven by stricter EU rules that are phasing down high-global-warming refrigerants and aiming to eliminate virgin HFCs by 2050. These changes are pushing the industry toward alternatives that have a much lower environmental impact.

One of the main alternatives is R-290 (propane), a natural refrigerant with a very low global warming potential that has already been used safely in millions of household refrigerators and is now increasingly used in heat pumps. Some manufacturers, including Daikin, now offer R-290 systems that can reach high efficiency levels and produce the higher water temperatures needed for older radiator systems.

Many European governments are also encouraging the shift with subsidies that can cover roughly 30–40% of installation costs. Combined with the move away from fossil fuels in building regulations, this trend means installing a heat pump today can help future-proof your home against tightening efficiency standards.

Maintenance and lifespan

Heat pumps are designed for long-term use, typically lasting between 15 and 20 years with proper servicing. This longevity, combined with lower running costs, can boost a home's energy performance rating and property value.

Annual professional servicing covers checking refrigerant levels, cleaning the heat exchanger coils, inspecting electrical connections, and testing the reversing valve. The logic is the same as servicing any refrigeration system: the components are identical, just at a larger scale.

Homeowners can support performance between services with a few straightforward habits:

  • Keep air filters clean, particularly during periods of heavy use. A clogged filter can noticeably reduce efficiency and increase running costs.
  • Clear debris and vegetation from around outdoor units to maintain good airflow.
  • Make sure indoor units are not obstructed by furniture or soft furnishings.

Maintenance costs and service contract options vary by country and system type. It is worth discussing ongoing support arrangements with your installer at the point of installation, since preventive care helps maintain efficiency and control energy costs over the system’s lifetime.

Conclusion: the same science, scaled for your home

The parallels between heat pumps and refrigerators show that heat pump technology is built on proven physics that has been working reliably in European homes for generations. Both achieve their results by moving heat rather than generating it, which is why a heat pump can deliver several units of heat for every unit of electricity consumed.

That efficiency translates into lower running costs, reduced dependence on fossil fuels, and the convenience of a single system that can both heat and cool your home. As building regulations tighten and electricity grids shift toward renewable energy, systems that run entirely on electricity are also becoming an important part of future-proofing residential heating.

Key takeaways

  • Heat pumps and refrigerators use the same four components: evaporator, compressor, condenser, and expansion valve. Both move heat rather than generating it.
  • A heat pump can deliver 3-4 units of heat for every unit of electricity consumed, which can help reduce household energy bills.
  • Unlike a refrigerator, a heat pump is reversible, meaning one system can provide both heating in winter and cooling in summer.
  • Modern heat pumps operate effectively in sub-zero temperatures thanks to refrigerants designed to absorb heat from cold outdoor air.
  • Natural refrigerants such as R-290 are increasingly used in new systems, helping homes adapt to stricter environmental regulations and lower-carbon heating.