Skip to main content

Simple ways to improve heat pump efficiency, lower energy bills and stay comfortable in every season

Heat pump efficiency depends on how well your system is designed, installed and operated. The biggest gains often come from simple adjustments: keeping flow temperatures low, improving insulation, using correctly sized radiators or underfloor heating, and applying smart controls to avoid large temperature swings.

When these elements work together, your heat pump delivers consistent comfort with lower energy use. In this guide, you’ll learn why efficiency varies between homes, what you can optimise yourself, and when to involve a professional to ensure the best performance all year round.

How does a heat pump work?

Unlike traditional heating systems, heat pumps do not generate heat but transfer it from one place to another, which makes them highly efficient.

Air source heat pumps extract heat from the outdoor air, even in cold conditions, and ground source heat pumps draw stable heat from the earth beneath your garden.

After heating has been absorbed by the refrigerant in the system, it is compressed using an electrically driven compressor and its temperature raised. The heat is then circulated around your home via radiators, underfloor heating or warm air systems.

What makes a heat pump efficient?

Heat pumps are efficient because they move heat rather than create it.

Key efficiency principles:

  • It requires much less energy to move heat than to generate it
  • It simply moves energy from the outdoors to inside instead of burning fuel or generating heat via resistance
  • It delivers long-term efficiency when properly designed, installed, insulated and controlled

A well-optimised system can provide consistent comfort with significantly lower energy consumption.

What does heat pump efficiency really mean? (SCOP explained)

Heat pump efficiency is typically measured using the Seasonal Coefficient of Performance (SCOP).

  • A SCOP of 4 means the system produces 4 units of heat for every 1 unit of electricity
  • However, this value is not constant — it changes depending on conditions, hour by hour

Efficiency depends mainly on the temperature difference between outdoors and your heating system. As a result, two identical heat pumps in two seemingly similar homes can perform very differently.

A house with poor insulation, draughty windows or high-temperature radiators loses more heat more quickly and forces the heat pump to produce much hotter water. Modern, well-insulated homes retain heat for longer, allowing the heat pump to run at lower, more efficient temperatures.

Heating habits also matter: large indoor temperature swings caused by frequently turning the heating up, down or off push the heat pump out of its optimal operating zone, whereas maintaining a steady, slowly varying temperature keeps it running efficiently.

SCOP reflects the expected seasonal performance of a heat pump across a full year of typical use and varying outdoor temperatures. This is why small changes to your settings or home — like improving insulation — can significantly impact efficiency and energy costs.

Why flow temperature is key to heat pump efficiency

Flow temperature, the temperature of water circulating through your radiators or underfloor pipes, is one of the most important efficiency factors in how efficient a heat pump will be.

Heat pumps perform best at lower flow temperatures, typically 35–45°C. Therefore the compressor consumes less electricity, delivers warmth gently and constantly to rooms, and keeps an even indoor temperature/heat distribution across all rooms.

When the required flow temperature rises toward 50°C or above, the compressor needs to work harder, increasing electricity use and reducing seasonal efficiency.

For a lot of houses, just lowering flow temperature by several degrees will make a big difference. A lot of installers suggest going down in these settings over a few days to see what the lowest comfortable point is. This keeps the heat pump running in its sweet spot, and discourages rapid cycling (frequent on-off cycles) that can occur from temperatures changing too quickly.

How to heat water efficiently with a heat pump

Hot water use is a more significant factor in heat pump efficiency than many homeowners realise. While conventional boilers often heat water to 60°C or higher, heat pumps operate far more efficiently when hot water is maintained at around 50°C for everyday use. Most households can shower, clean and do dishes comfortably at this lower temperature, reducing the load on the system and lowering energy consumption.

Some systems still run periodic “boost” cycles to temporarily raise water temperature for hygiene purposes. These are normal, but you can optimise efficiency by scheduling them during off-peak electricity hours and by aligning them with space heating cycles.

Because hot water demand is relatively predictable (based on household size and routines), reviewing when and how you use hot water helps ensure it is heated efficiently and only when needed.

How smart controls improve efficiency

Weather compensation is one of the most effective ways to improve efficiency while maintaining comfort. It automatically adjusts the flow temperature based on outdoor conditions.

Instead of running at a constant temperature:

  • On mild days, the system lowers water temperature without affecting comfort
  • On colder days, it increases output only as much as needed

This prevents one of the biggest efficiency losses: unnecessarily high flow temperatures.

When combined with a smart thermostat, the system learns how your home responds to temperature changes and builds a heating curve over time. It figures out, over time, how long your home takes to heat up and cool down based on weather. This cuts down on needless cycling, maintains an even temperature overall, and makes the heat pump more efficient.

How underfloor heating optimises efficiency

Underfloor heating works exceptionally well with heat pumps because it operates at lower water temperatures and distributes heat evenly across a large surface.

Key benefits include:

  • Operates efficiently at 30–40°C, ideal for heat pumps
  • Provides gentle, even heat distribution
  • Maintains stable indoor temperatures
  • Reduces on/off cycling by releasing heat slowly over time

Because the system delivers heat steadily rather than in bursts, the heat pump can run more consistently at low power — which is its most efficient operating mode.

Adapting radiators to low temperature systems

Radiators can still work effectively with heat pumps, but they must be able to deliver sufficient heat at lower flow temperatures. In homes originally designed for boilers (70–80°C systems), existing radiators may struggle to warm the room unless the flow temperature is raised by making some adjustments.

Possible adaptions include:

  • Upgrading to larger or low-temperature radiators
  • Using high-output aluminium models for better heat transfer
  • Replacing radiators in the coldest rooms first
  • Choosing a heat pump that is designed to work at high temperatures

For central heating systems, this can be addressed by upgrading radiators in crucial rooms. Bigger radiators, or new low-temperature ones, have a larger surface area for heat exchange so they can provide the same level of comfort at lower temperatures. High-output designs (even with aluminium models) warm up and cool down more slowly to maintain an even environment throughout the room. Even swapping just one or two radiators in the chilliest parts of the home can help improve the overall efficiency of the system.

Why proper heat pump sizing matters

Correct sizing is also critical for both efficiency and comfort. An oversized system can generate heat faster than the home can absorb, resulting in repeated on/off cycling that wastes energy and wears out components prematurely. An undersized system may run constantly in cold weather and fail to make it comfortable.

Proper sizing is based on your home’s heat loss, not just its size. When correctly matched, the heat pump can run for longer periods at low power — exactly how it achieves maximum efficiency.

Why is commissioning as important as installation of a heat pump?

Installation is only part of the process. Commissioning, configuring and adjusting the system ensures the system performs as intended.

During commissioning, installers will:

  • Adjust flow rates
  • Set heating curves for weather compensation
  • Balance radiators or underfloor loops
  • Programme heating and hot water schedules

These measures help to guarantee that the heat pump is working properly.

Incorrect commissioning can significantly reduce efficiency. For example, if flow temperatures are set too high or radiators are not properly balanced, the system may underperform—even when using high-quality equipment.

Regular check-ups help maintain performance and identify small adjustments that can significantly improve comfort and running costs.

How home insulation improves heat pump efficiency

Insulation is one of the biggest drivers of heat pump efficiency. Heat pumps work best when they can meet demand with low flow temperatures, which is only possible if heat is retained inside the home.

Improvements such as:

  • Loft, wall and floor insulation
  • Draught-proofing
  • Upgraded windows and doors

help create a more stable indoor environment, reducing the workload on the heat pump.

Even small improvements — like sealing gaps or insulating pipework — can allow you to lower flow temperatures further, reducing energy use while maintaining comfort.

Using solar energy and thermal storage to increase efficiency

Combining a heat pump with solar energy can significantly improve cost-effectiveness and increase the share of renewable energy you use.

  • Photovoltaic (PV) panels generate electricity to power the heat pump, and that can directly be used to power the heat pump or stored in a battery at homes.
  • Solar thermal systems can pre-heat domestic hot water, reducing the load on the heat pump and shortening reheating times.

Thermal storage adds flexibility by storing energy for later use. For instance, they could enable the system to capitalize on cheap electricity prices at off-peak hours or hold onto self-generated solar energy. These integrations are not necessary for the operation of a heat pump, yet they can bring down your energy bills and boost the portion of renewable energy you use in your house.

How to reduce heat loss within your heating system

Heat loss doesn’t only occur through walls and windows — it can also happen within the system itself.

Exposed pipework in lofts or garages can lose heat before it reaches radiators or underfloor pipes. Insulating pipes ensures heat is retained within the system, which means using less energy to keep you at a comfortable temperature.

System components also matter. Variable-speed circulation pumps reduce unnecessary electricity use by adjusting their speed based on demand. Older, fixed-speed pumps may run at full power even when it’s not needed, wasting electricity.

In some setups, a buffer tank can help reduce rapid cycling, allowing the heat pump to operate more smoothly and increasing both efficiency and lifespan.

Zoning and everyday control habits

Efficiency is directly affected by how you control your heating system. That’s because heat pumps work more efficiently when they can sustain a steady temperature, rather than reacting to large fluctuations.

Zoning your home (dividing it into areas that can be separately controlled for heating) lets you heat only the rooms you are using and adjust temperatures based on the time of the day. For instance, living spaces might require more heat in the evening, whereas bedrooms often don’t need as much during daytime hours.

Zoning is even more convenient with smart thermostats that learn your habits and adjust themselves automatically. They can take the chill off rooms by pre-heating them gradually, provide gentle background warmth without waste and avoid erratic blasts of high-intensity heat.

Incrementally changing setpoints by one or two degrees, rather than large jumps, also allows the heat pump to remain within its most efficient operating range.

Efficiency in cold weather and defrost cycles

In cold, damp conditions, air source heat pumps may develop frost on the outdoor unit. To manage this, the system runs defrost cycles, temporarily reversing operation to clear ice. These cycles are normal but can slightly impact efficiency. These cycles are perfectly normal and essential, however their frequency and duration impacts performance. To minimise their impact you should keep the outdoor unit clear of snow and debris and ensure proper airflow around the unit.

Maintaining a steady indoor temperature is also key. Large temperature swings force the system to work harder and reduce efficiency. Heat pumps perform best with consistent demand, especially in winter.

How electricity tariffs affect heat pump running costs

While tariffs don’t affect how your heat pump operates, they strongly influence running costs. Houses with heat pumps can particularly benefit from time-of-use tariffs, which charge more only at certain hours. With some programming or settings changes, your system could be adapted to use the cheaper energy and take it into sustained use for heating water, running pumps, charging radiators or pre-warming a house before electricity prices rise.

Smart controls, thermal storage and well-scheduled operations make it easier to shift energy consumption without sacrificing comfort.

Even without dynamic tariffs, avoiding repeated high-demand spikes - like ramping up the system over and over again - helps reduce strain on the system and improves long-term efficiency.

When to fine-tune your heating system

Your heating system should evolve as your home does. You should review your system:

  • After renovations, such as adding insulation, converting a loft, extending your home or replacing windows
  • If the system is several years old, it may benefit from recalibration of its settings in order to run efficiently

A professional check-up every few years can uncover simple but effective improvements such as:

  • Adjusting the weather compensation curve
  • Rebalancing radiators
  • Reducing the flow temperature
  • Upgrading radiators or other emitters

These adjustments are often low-cost but can deliver significant efficiency gains.

Conclusion

Maximising heat pump efficiency isn’t about complex technology — it’s about how your home and system work together.
By focusing on low flow temperatures, proper insulation, suitable emitters and smart controls, you can significantly reduce energy use without compromising comfort.
Regular optimisation and small adjustments ensure your system continues to perform efficiently throughout its lifetime.

Key takeaways

  • Lower flow temperatures are key to maximising efficiency and comfort
  • Radiators and underfloor heating must suit low-temperature operation
  • Good insulation reduces heat loss and improves performance
  • Smart controls and steady heating prevent energy waste
  • Regular system checks keep performance aligned with your home